Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an INF2 [Internal Error 2] fault on an ATV340 series drive and how do I correct it?

Article available in these languages: Spanish

Issue:
Customer is experiencing an INF2 [Internal error 2] Fault on an ATV340 series drive.

Product Line:
ATV340

Environment:
All

Cause:
The power board is incompatible with the control block software.

Resolution:
Contact your local Schneider Electric representative.