Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an INFA [Internal Error 10] fault on an ATV340 series drive and how do I correct it?

Issue:
Cause of INFA [Internal Error 10] fault on an ATV340.

Cause:
The input state is not operating correctly.  The internal drive thermal sensor is not operating properly.

Resolution:
Cycle power to clear the fault.

**

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)