Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is an INFb [Internal Error 11] fault on an ATV340 series drive?

Issue:
Customer is experiencing an INFb [Internal Error 11] fault on an ATV340 series drive.

Product Line:
ATV340

Environment:
All

Cause:
The internal drive thermal sensor is not operating correctly.

Resolution:
Cycle power to clear the fault.  If the fault returns, contact your local Schneider Electric representative.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)