Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Accessing specific web pages in a 170ENT11001 Ethernet Communication adapter will cause it to reboot
Issue
Accessing the 170ENT11001 web pages ‘Ethernet Statistics’ or “Momentum IO Values” using browsers with Java V1.8 will cause the adapter to reboot.

Product Line
Momentum - 170ENT11001 Ethernet Communication Adapters at SV 1.10 or higher.

Environment
  • Web browsers with Java version 1.8.
  • 170ENT11001 Web firmware version 1.03 (the web version number is found on the 'Home' page after login)

Resolution
  • Installing web firmware version 1.04 into the 170ENT11001 resolves the adapter reboot issue.
    Reference web page filename: 170ENT11001_Web_V1.04.7z
  • This file is not for use on 170ENT11001's with an SV less than 1.10.