Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use a Vijeo Designer recipe object from the Webgate ?

Issue:
There are certain limitations while using Recipe objects in Web Gate.

Product Line:
XBTGT
HMIGTO
HMIGTU
IPC with VJD Runtime

Environment:
Vijeo Designer V6.2

Resolution:
The Data Sharing for the recipe control variable (_RecipeControlDefault) must be set to None.
Also the Internal Recipe variables associated to the ingredients must be set to none.
The external Recipe variables associated to the ingredients can be set to Read/Write.





Schneider Electric Saudi Arabia

Attachment(s)
RecipeControlDefault.jpg [211.01 KB]
Recipe.jpg [176.28 KB]
RecipeInternalVariables.jpg [91.86 KB]