Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference in Digital inputs and Logic inputs on the ATV320 drives?
Issue:
Difference in Digital inputs and Logic inputs on the ATV320 drives

Product Line:
ATV320

Environment:
Logic inputs

Cause:
n/a

Resolution:
They are the same thing. In older drives, we always used logic inputs and with the newer drives, we are calling them digital inputs. They are exactly the same thing.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre