Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for a mounting adapter to replace an ATV61/71 with an ATV630/930?

Issue:
What is the part number for the substitution kit for ATV61/71 to ATV630/930?

Product Line:
ATV630 ATV930

Environment:
ATV630 ATV930

Cause:
Replacing ATV61/71 with new ATV630/930.

Resolution:
The part numbers for the mounting adapters are selected based on VFD frame sizes. These kits are used to install an Altivar Process Drive in the place of an Altivar 61 or Altivar 71 drive, using the same mounting holes. It includes the mechanical adaptors required for mounting.
See attachment.

Schneider Electric Saudi Arabia

Attachment(s)
Mounting plate convert 61-71 Process MFR22528.pdf [169.62 KB]