Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can Lexium 28 be controlled via Modbus RS485 ? Revision 2

Full Modbus control of LXM28 is not possible because Modbus control words are not part of the firmware design.

However, it is possible to read and write parameters via Modbus
This means it is possible to create motion via Modbus however full control the drive via the Modbus channel is not possible
This is due to the fact that there are no Modbus objects available on LXM28 for the "ControlWord" and also no control words available for the "ModesOfOperation" via Modbus.

It is possible to create some simple motion using Modbus because it is possible to write via Modbus and activate the digital inputs on and off, this is covered in the attached PDF file.

Customers looking to control LXM28 via Magelis will need to choose a model that supports integrated CANopen master, (such as XBTGC or SCU) to control LXM28 via Magelis.

Magelis such as XBTGC and SCU are implemented into SoMachine and therefore the LXM28-PLCopen Library can be used.


See the attached PDF file which covers simple control of Lexium 28 via Modbus.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
Modbus Control of LXM28.pdf [1.03 MB]