Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the MN suffix mean on an ATV630 or ATV930 drive part number?
This pertains to the frame size 7 Altivar Process drives, which have the option to add the "MN" suffix.
This indicates that the VFD is supplied without a DC Choke.
If MN is not included on a part number, the DC Choke is included.


If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)