Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION8800 energy test results
Issue
ION8800 conformity test with IEC 62052-11 and IEC 62053-22/23 standards by KEMA

Product Line
ION8800

Environment
Test

Cause
The energy meters were tested in respect of the following requirements:
-  IEC 62052-11 (2003): Electricity metering equipment (a.c.) - General requirements, tests and test conditions - Metering equipment.
-  IEC 62053-22 (2003): Electricity metering equipment (a.c.) - Static meters for active energy (classes 0,2S and 0,5S)
-  IEC 62053-23 (2003): Electricity metering equipment (a.c.) - Static meters for reactive energy (classes 2 and 3)

Resolution
Refer to attached document.

Schneider Electric Saudi Arabia

Attachment(s)
ION8800_KEMA_IEC62053_EnergyTest.pdf [4.5 MB]