Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which ATV320 drives are supplied with an EMC plate?

Article available in these languages: Spanish

Issue:
EMC Plate on ATV320 Drives.

Product Line:
ATV320, Altivar Machine

Environment:
Altivar

Resolution:
See the attached excerpt from the catalog.  Subnote 6 identifies the models that include the EMC plate.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
ATV320 EMC plate.pdf [348.99 KB]