Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Altivar 320 Variable Speed Drive: Programming a Flashing Output Signal Using Logic Functions

Article available in these languages: Czech

Using 2 timers it is possible to program a flashing signal.
Min setting is 0.1second up a level, 0.1second down a level.
See Altivar 320 logic in the attachment.
The output of the logic is connected to relay output (for test only)
The first timer defines period of the signal, second timer defines duration of the signal up a level

Schneider Electric Saudi Arabia

Attachment(s)
Flashing signal.jpg [42.73 KB]
ATV_flashing_signal.zip [2.12 KB]