Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What for are SMIL and SMAL parameters in ATV drives?
The meaning of parameters SMIL and SMAL is the same as LSP and HSP. SMIL/SMAL is in rpm (and it is according to cia402 standard), LSP and HSP is in Hz. When SMIL and SMAL is changed, LSP and HSP is changed automatically to corresponding values and vice versa.