Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to solve the issue that Unity Pro XLS V7 will crash if any action made in Win7 SP1.

1.Issue

Customer are using Unity Pro XLS 7.0 for developing logic with Quantum safety controller. The software was installed in a laptop with Windows 7 SP1 Operating system and was having 16GB RAM. The Unity Pro application was opening but if customer do any action like saving or analyzing project, the software crashes immediately and closes with a message as attached.


2.Environment

Windows 7 SP1, Unity Pro XLS V7.

3.Resolution

Uninstalling the Microsoft visual c++ 2012,2013,2015 Redistributable (x64) (x86) all these from PC in “Programs and Features”, then re-install the unity pro XLS 7.0.
C++.png

4.FAQ Applicable Conditions (Optional )

No.

Schneider Electric Saudi Arabia

Attachment(s)
Remove C++.PNG.png [25.52 KB]