Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to create a color animation in Vijeo Designer that displays for specific and non-sequential values only?

Issue:
Create a color animation in Vijeo Designer

Product Line:
Vijeo Designer

Resolution:
In order to create a color animation that only displays for specific values in Vijeo Designer, you will need to use a Color Animation object, such as a Circle or Rectangle.
Follow this procedure below to setup the object:

1) Draw a Circle object
2) Double click on the Circle and select the Color Tab
3) Set the Mode as "By State"
4) Set the Data Type as "Integer Types"
5) Beside Value List, press the [...] button to open the Value List dialog
6) Map the individual states to the values that you need to use. (ex State1=10, State2=12, State3=19)
7) Create a Color Animation for your X number of states by creating a new resource directly from the object.
8) Assign the Color resource to the object.

With the setup above, at runtime, we will be able to display a different color for each value specified in the Value list.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre