Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In EcoStruxure Machine Expert, how do I set up the Gateway for downloading my PLC application to a device with a specific Subnet Mask?

Issue

In EcoStruxure Machine Expert or SoMachine v4.3, how do I set up the Gateway for downloading my PLC application to a device with a specific subnet mask?

Product Line

EcoStruxure Machine Expert, SoMachine v4.3

Environment

Configuration Software for Windows

Resolution

To set up the Machine Expert Gateway to be able to connect to devices with a specific subnet mask (in this example, '255.255.255.0'), follow these steps below:

  1. Run Notepad.exe as Administrator in Windows
  2. From Notepad, open the file "Gateway.cfg" in the SoMachine Gateway folder (default location: "C:\Program Files (x86)\Schneider Electric\EcoStruxure Machine Expert\Tools\Gateway")
    (For SoMachine, the location is "C:\Program Files (x86)\Schneider Electric\SoMachine Software\Tools\Gateway\")
  3. Under the [CmpBlkDrvUdp] section, add the line "itf.0.networkmask=255.255.255.0" (or replace 255.255.255.0 with a subnet mask of your choice)
  4. Save the Gateway.cfg
  5. Restart the Gateway Service from the green "=S=" logo icon on the right side of the Windows taskbar (or restart the Windows Service called 'CoDeSys Gateway V3')

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:

Need help?

  • Product Selector

    Quickly and easily find the right products and accessories for your applications.

  • Get a Quote

    Start your sales enquiry online and an expert will connect with you.

  • Where to buy?

    Easily find the nearest Schneider Electric distributor in your location.

  • Help Centre

    Find support resources for all your needs, in one place.

  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre