Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can we make a numeric display with an expression also have input in Vijeo Designer?

Issue:
Numeric display with an expression also have input

Product Line:
Vijeo Designer

Resolution:
In Vijeo Designer, a numeric display with an expression cannot have input activated. In order to achieve this, you will need to make your own custom object using the following:
1) A numeric display with the expression.
2) An invisible switch.
3) A numeric display with input activated.

This example assumes that the numeric display with the expression only involves one tag.

The idea behind this setup is that we will use visibility animation to show and hide the appropriate numeric display. In a normal mode, we will display the numeric display with the expression. The visibility condition for this numeric display should be assigned to a boolean call "Hide_Display" for example. The expression for the Visibility condition should be "!Hide_Display."

Next, the invisible switch will be used to set to the boolean. Therefore the operation is the Bit Set operation on the boolean "Hide_Display". In addition, the visibility condition is also set to "!Hide_Display".

Finally, the numeric display with the input activated should have Visibility set to "Hide_Display" so that when the boolean is High, it is displayed while the other is hidden. In the Advanced tab of the numeric display, we should also set the "Use Input Trigger" and "Input Status Variable" to "Hide_Display". The status mode should be set to "ON/OFF Reverse Mode". These settings will allow the boolean to be reset after an number is entered.

Please see the attached example for a demo.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia

Attachment(s)
Example.zip [20.35 KB]