How can we help you today?

How to run Modsoft in Windows 10.

Issue
How to run Modsoft in Windows 10.

Product Line
Modsoft

Environment
Windows 10

Resolution
Modsoft is considered to be obsolete.  There is no longer any Engineering support for the product.  It is recommended to update to either 'ProWORX 32'
or 'Control Expert'.

Modsoft is a DOS based program.  In order to run Modsoft in Windows 10, the PC will need to have either

  • A DOS emulator
  • NTVDM.dll installed.
  • Windows XP running in a virtual machine.


The following articles can be referenced on running a DOS based program in Windows 10.

https://www.howtogeek.com/228689/how-to-make-old-programs-work-on-windows-10/

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation