Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ION setup latest revision

Issue/Background:

Previously, updates were released in a Box folder, and ION Setup could check if the user had the latest version. Due to a change in policies, Box.com is no longer used by Schneider.

Product Line
ION Setup

Resolution
To provide a static, public-facing link that does not require individual authentication for ION Setup, the following URL will host the latest release:

https://www.se.com/ww/en/download/document/ION_Setup_Latest_Release/.

Using the ION Setup software available from this link, the tool can compare the user’s current revision with the latest release and determine if an update is needed. This resolves the issue of being unable to upgrade automatically at startup or manually within the tool.