Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can VW3A3501 controller inside card be used with today's ATV71 and to contorl ATV320 via Canopen?
Yes, controller inside card VW3A3501 is still compatible with ATV71 drives.
Bear in mind that programming of CI card used Codesys software and we cannot guarantee its operation on win 7 or win 10.
We recommend to use windows XP.
For connecting PC to CI card, you can use TCSMCNAM3M002P cable.

Do not forget to check battery in CI card and replace it because after long time it can be discharged.