Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the CFF fault on the ATS22 soft starter and what causes it?
Issue:
ATS22 soft starter getting a CFF fault code.

Product Line:
Altistart 22

Environment:
All

Cause:
N/A

Resolution:
This is an invalid configuration on power up error.
It can happen due to a corrupted SoMove file download or MultiLoader tool.
Please revert to the factory settings under UTIL menu.
https://www.se.com/us/en/faqs/FA175288/