Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Easergy Micom P643 relay is displaying RTD board fail .Whether this affect the relay’s function ?

Issue/Description :

An alarm "RTD board fail" message displayed in the Easergy Micom P643 relay

Product family:

Easergy Micom P643 relay

Resolution:

As per our manual, In the case of an RTD board failure, an alarm "RTD board fail" message will be displayed, the RTD protection disable during this time
but the operation of the rest of the relay functionality is unaffected.