Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to properly calibrate the touchscreen on a HMIBMU series
Issue:
The touch screen calibration is still inaccurate even after using the Windows Control panel's Tablet PC Settings.

Product Line:
Magelis iPC, HMIBMU, HMIBMI

Resolution:
When calibrating the touchscreen of an HMIBMU or HMIBMI series, ensure not to use the Windows calibration tool. Instead, look for the PenMount Control Panel and use the calibration tool of that application. It provides the option for 25 points of calibration. By using 25 points, it gives the touchscreen a more accurate calibration.