Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to mitigate Unity Pro Resolution issue ?
The pad resolusion on unity pro screens is related to the windows resolution if the windows layout size is 100%, unity text is small and barely readable.
Set your windows scaling to the Recommended value (150% or 125% based on your machine).
>>> Right click on the desktop …… Select display setting ……. At change the size of text, apps, and other items ----- select the recommended scale ……….. At Resolution-----select the recommended resolution.