Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to modify runtime security setting on EOTE V3.1 with USB drive
1. Issue
How to modify runtime security setting on EOTE V3.1 with USB drive
2. Environment
EOTE V3.1
3. Resolution
  1. ) Set In the [Project Explorer], select [Security] [Setting], and click [Export].
  2. ) Define the location and file name.
Note: To import the exported file to the panel, save the file to the root directory of USB   memory with the specified folder and file name.
Folder Name:  UserManagement
File Name: data.bin
3. )   Enter the encryption key. This key is used for importing and modifying user information.
4. )   To import user information from the panel, setting up scripts is required.
5. )   On the screen, touch the import switch.
6. )   Enter the encryption key. On the panel, the project user information is overwritten.
4. FAQ Applicable Conditions
FAQ also applies to Vijeo XD V3.0.