Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
I have TAC I/NET Access Control system, How can I migrate to EcoStruxure Security Expert?
With the new available upgrades, existing TAC I/NET access control customers can be easily migrated to EcoStruxure Security Expert. By transitioning, they are migrating their existing access control systems to an IT-friendly, integrated access control solution.

Database Transition:

EcoStruxure Security Expert provides native connectivity to TAC I/NET access control
systems. The existing I/NET system databases can be easily synchronized using the Security
Expert data synchronization service, SX-DB-SYNC, saving hours of extensive engineering time by avoiding the
need for staff to re-program their current systems.  The INet Database Transition Tool retrieves data such as DCUs, doors and individuals from an INet database.

Transition a controller level:

The TAC I/Net door and IO modules are natively supported in the Security Expert controller, SP-C. The SP-C replaces Xenta527 and iSite subLAN controllers 7798C in I/NET access control transitions, while maintaining full system level functionality over existing installed bus topology. We recommend using NetSys NV202 VDSL2 LAN extenders to extend Ethernet over existing RS485 wiring, if required, in the transition architecture.
TAC I/NET Modules supported:
• DPU7910
• DPU7920
• SCU1200
• SCU1280
• SCU1284
System architecture – TAC I/NET transition to Security Expert
Machine generated alternative text:TAC I/NET Data Synchronization Service Ethernet ' NV202 Xenta527 IP over ekisting twisted\pair • Etherqet iSite7798 sp_psu 12VDC SP-C SCU/DPU 10 mod. iSite 1 subLAN Security Expert To next iSite on Xenta RS485 SCU/DPU 10 mod. iSite 2 subLAN & RS485 field bus Last iSite on Xenta RS485 Sp. SCU/DPU 10 mod. U) iS1te n subLAN Up to 32 (max) SCU/DPU devices persubLAN Support for existing I/NET features
Note: You can find the Transition tool and more information at the Exchange:
https://ecobuilding.schneider-electric.com/search#keyword/INET Security Expert/tab/documents