Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I change the relay status from NO to NC on the Altivar Process Drives?
Issue:
They need to change the function of the output relay from Normally Open contact to a Normally Closed contact.

Product line:
Altivar Process, ATV600 ATV900

Environment:
all

Cause:
The Altivar Process drives come with only R1 having a normally open and normally closed contact.  R2, R3 and the extended IO Card relays are all Normally Open only.

Resolution:
Under the Relay configuration menu (i.e. R2 Configuration > go to R2 Active at.  The factory setting is 1 (closed).  Change this value to 0 for active when open to invert the relay output signal.

NOTE:  Operating State Fault (FLT) cannot be assigned to 0.  If an additional NC contact is needed for Fault indication, add an external control relay with the additional contacts.