Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many built-in RJ45 communication ports are in an ATV630 drive?

Issue:
Number of RJ45 communication ports on a standard ATV630 drive

Product Line:
ATV630


Resolution:
The ATV630 has 2 built-in RJ45 communication ports as standard:
1 Ethernet Port (TCP only)
1 Modbus Serial Port

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)