Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to activate Motor analog PTC in TeSys T (LTMR) using SoMove?

The PTC Analog motor temperature sensing function is enabled when the Motor Temp Sensor Type parameter is set to PTC Analog and the LTM R controller is connected to an analog PTC thermistor embedded in the motor.

1

The PTC analog motor temperature sensor function has the following configurable parameter settings:
Fault thresholds setting range 20....6500 ohms

2


Warning thresholds setting range 20....6500 ohms

3

However, this value needs to be set as per the motor/thermistor specifications.