Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between SmartX server embedded client licenses and Windows client licenses?

The availability of embedded licensing, starting from EBO V3.0, will permit the addition licensing enforcement at the SmartX Servers, AS, AS-P and AS-B.

EBO 3.1 builds in the removal of any need to activate a Client feature license on SmartX servers to be able to connect WebStation to a SmartX server and log in. Where 3.0.4 and 3.0.3 with hot fix accomplished the same functionality, they did so by stating that 99 clients were available. In version 3.1.1 there is simply no checking for Client feature licensing, and there is no claim for any specific number of clients.

In order for WorkStation to operate it must have access to a Windows license on a PC that is running a Windows OS. Since WorkStation software requires a Windows operating system, then the license might be installed on the same PC or it might make use of a demo license.