Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Geo SCADA - Local ViewX Client Activation

This article shows the correct way of licensing the local ViewX client by using the client license method :

LicenseDetail

As per the previous screenshot, the number of "ViewX Clients"- in this example - is Zero. This means you will not be able to activate remote clients connected to this server unless purchasing a separate valid license, However you can activate the local ViewX client that is installed in your local machine hosting your Geo SCADA server.

Please follow these steps :

  1. Click the Windows Start Menu, highlight EcoStruxure Geo SCADA  and select Configure Connections.
  2. Click on the 'Properties' button from the right side and make sure that your Geo SCADA Client Configurator has the "Use Client Licensing" option is checked, Then click Ok

    ClientInformation
  3. Back to The Geo SCADA Exper 'Client Dialog' again - Click on the 'Licenses' button:

    ClientLicense1
  4. The following screen will appear:

    ClientLicensing
  5. Click the browse button and browse to the same file used to activate the server.
  6. Select file and click open.
  7. Click on "Apply". The license mode should now show as "File based client license" and validity is "valid".
  8. Click on the OK button and close the 'Client Licensing' dialog.

    licValidation
  9. (Re)start the ViewX client by clicking the ViewX icon on your desktop.

    Note : If the Machine ID does not appear in Step 4 or Step 8, make sure the Geo SCADA License
    Server service is running.

Geo SCADA Expert lic