Lighting can be connected to HRC as shown in the following architecture, Consider the following:
- Lighting on/off control, the use of 230VAC relay is a must.
- For dimming, the current HRC only supports 0-10V. However, there may be cases of compatibility issues for certain dimming drivers, and therefore, it is recommended to test the compatibility in advance. In case of compatibility issues, adding a resistor (600Ω, 0.5W) in parallel with the dimming drive may solve the issue.
Released for: Schneider Electric Saudi Arabia