Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to connect the computer to EVlink Parking and access the commissioning tool?
Computer configuration
  • Check that your computer is physically connected to the charging station and that it is powered on.
  • Open the local network properties menu of your computer.
  • Open Internet Protocol TCP/IP v4 properties.
  • Set the static IP address properties as follows:
    • IP address: 192.168.0.x (where x is a number between 241 and 249)
    • Subnet mask: 255.255.255.0
    • No default gateway
    • No DNS server
    • No proxy
Logging on to the Commissioning tool
  • Open a web browser and type http://192.168.0.102 in the URL field.
  • On the Login page, choose the language, and complete the User name and Password fields. The factory settings appear below.
  • Click Login: if the user name and the password are correct, the commissioning home page appears.
Otherwise, an access refusal message appears.



Know more about Electric Vehicle (EV) Charging