How can we help you today?

Can ARGUS Presence detector P/N CCT551011 be installed at a height of 3.2 meters?

P/N CCT551011 is an ARGUS Presence detector with Dual Technology featuring PIR (Passive Infra Red) and Ultrasonic detection. Although it is recommended to be installed at a height of 2.5 meters to gain optimal detection pattern, it can be installed at the height of up to 3 meters. If installed at 3.2 meters, the detection area will slightly increase and the sensitivity will slightly decrease as the distance between segments would be larger and thus the user will have to move a slightly longer distance to cut more than one segment of the presence detector and as a result the lighting regulation might not be the most optimum.

Generally, the sensors depending on PIR and Ultrasonic technologies are recommended to be installed at a height of 2~3 meters to guarantee best performance. We do not have sensors with these technologies that could support higher heights without affecting the sensing performance.

On the other hand, we can reach heights of 10 meters using Argus Presence Detector P/N CCT551023 which depends on high frequency detection technology instead of PIR and Ultrasonic detection technology.

You can also find the instruction sheets for P/N CCT551011 and P/N CCT551023 at the links below:
Instruction sheet for P/N CCT551011: https://download.schneider-electric.com/files?p_enDocType=User+guide&p_File_Name=CCT551011_CCT551012_HW_2016_38_EN_ZH_FR_DE_TR_NO_SV_RU_NL.pdf
Instruction sheets for P/N CCT551023: https://download.schneider-electric.com/files?p_File_Id=8856706911&p_File_Name=CCT551023_HW_2016_38_EN_ZH_FR_DE_TR_NO_SV_RU_NL.pdf

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: