Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why do some old Quantum I/O modules randomly go to fallback mode when communicating with 140CRA31200 (Ethernet) drop head
This is due to the fact that old components used in IO manufactured before 2008 are more stringent in regards to the internal timing specifications with CRA.

As we could not redesign the "old" IO modules that exist in the field already, the correction is applied in the 140CRA31xxxx .

This correction is embedded in PV06 or later versions of 140CRA31xxxxx

Schneider Electric Saudi Arabia

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: