Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum voltage per pole for iC60, C120, NG125 and C60H-DC?

The C60 (or iC60) offers are compliant with 60V DC per pole.
C120 / NG125 offers are compliant with 125V DC by pole
C60H-DC offer is compliant with 250V per pole.