Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the path of the Data Location designated as Main Drive in Vijeo Designer v6.2 Runtime on Magelis iPC?
Issue
In Vijeo Designer HMI configuration software's Data Location settings, one can define where data such as the User Application, Data Files, Forms, Recipes, and Web Server are stored.
On a Magelis iPC running Vijeo Designer Runtime software, where is the file location of the "Main Drive"?

Product Line
Vijeo Designer v6.2

Environment
Windows Embedded Standard (based on Windows 7) or Windows 10

Resolution
The file folder location path of the "Main Drive" is:
C:\Program Files (x86)\Schneider Electric\Vijeo-Designer 6.2\Vijeo-Runtime\Public\Projects\<ProjectName>\

This can be the storage location for data such as the User Application, Data Files, Forms, Recipes, Web Server (for Web Gate) as defined by the Options->Data Locations settings:
Data Locations settings