Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why is ramp stop the only option for the Type of Stop (Stt) on the ATV320 drive?

Issue:
On ATV320 drive, only ramp stop can be assigned to Type of Stop (Stt).

Product line:
ATV320

Environment:
All serial numbers

Cause:
Customer wanted to assign Freewheel Stop.

Resolution:
If the brake logic function (bLC) has been enabled or if Low speed time out (tLS) is not 0, then the Type of Stop (Stt) parameter is forced to Ramp Stop..