Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the type of web browser used by EBO WorkStation to present hyperlinks?
The EcoStruxure Building Operation software supports hyperlinks. Hyperlinks can be added and displayed in WorkStation. Hyperlinks can also be added in, for example, a graphic that is displayed in WorkStation. In WorkStation, you can navigate on the web page in the same way as in a web browser.

The EcoStruxure Building Operation software uses Microsoft Internet Explorer to present web pages. Plug-ins, for example, Flash and Java, have to be installed to be able to correctly display pages that use these plug-ins. If you have an issue in displaying a hyperlink in WorkStation, you shall make sure that it is supported by Internet Explorer and working there correctly.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre