Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the equivalent function in Vijeo XD 3.1 to Vijeo Designer?

** What is the equivalent function in Vijeo XD 3.1 to enable the visibility blinking function (Show/Hide/Blink Speed) for any object?
EOTE
It is not possible to directly enable the Blink Animation in EOTE. Only the Visibility Animation.
**What is the equivalent function in Vijeo XD 3.1 to enable Reference string (%Variable name%)?
No equivalent function in EOTE v3.1. Consider adding in V3.2, which is scheduled in Q2 2020.

**What is the equivalent function in Vijeo XD 3.1 to Create Objects with Variable Placeholders ($Variable name$)?
No equivalent function in EOTE v3.1. Consider adding in V3.2, which is scheduled in Q2 2020.

**What is the equivalent function in Vijeo XD 3.1 to Create linked Objects?
No equivalent function in EOTE v3.1

**What is the equivalent function in Vijeo XD 3.1 to create my own Tool chest?
No equivalent function in EOTE v3.1

**What is the equivalent function in Vijeo XD 3.1 to Create a project user list and Add/Remove from Runtime window?
EOTE
Can Add/Remove User Group and User from this page.
**What is the equivalent function in Vijeo XD 3.1 to Create Objects with Value animation (#)?
No equivalent function in EOTE V3.1
** What is the equivalent function in Vijeo XD 3.1 to enable the Hold delay function?
EOTE
This function can be achieved using screen scripts.

**Where can I found the download link for SP1 of Vijeo XD 3.1?

The download link will be provided when EOTE V3.1 SP1 is officially released (2019 October)