Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to perform a factory reset on the Altivar ATV320 drive?

Article available in these languages: Greek

Issue:
How can I perform a Factory Reset on the ATV320 drive.

Product Line:
Altivar 320

Resolution:
To perform a factory reset from power up:
Enter on dial
Scroll to CONF menu and enter
Scroll to FCS- and enter
Scroll to FRY- and enter
Select All so that " mark is at top instead of bottom
Now go to GFS parameter
Set it to YES and hold enter for 2 seconds until display LEDs stop flashing
VFD is reset to factory defaults