Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to delete recipes at runtime on the Magelis HMI?

Issue:
Looking for options on how to delete recipes created or downloaded to the Magelis HMI at runtime.

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, there are a couple of ways in which we can delete a recipe during runtime on the Magelis HMI.

The first option is to make use of a "Delete" recipe button that you can drag onto the panel from the toolchest in Vijeo Designer. During runtime, when you select a recipe group and recipe, when you press the Delete button, it will delete the selected recipe from the list.

The second option is to write a script in an action or in a touch action script. The script will essentially write a value to the _RecipeDefaultControl.Operation variable. The value to trigger a delete is the value "16"

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)