Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there an alternative part for the HMIZGAUX?

Issue:
The lead time for the HMIZGAUX is quite substantial. Looking for an alternative part number for the same part.

Product Line:
Magelis HMI (XBTGT, HMIG3U, HMIG3X, HMIG5U, HMIG5U2)

Resolution:
If the lead time for the HMIZGAUX is too long, consider checking your suppliers for Phoenix Contact's equivalent part of: FK-MC 0.5-2.5 7 position. (1908114)

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)