Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to clear the SD Card Error on the BMXNOE0100?

Issue:
I'm seeing the SD Card Error LED on solid on the BMXNOE0100. How can I clear this error?

Product Line:
M340

Environment:
EcoStruxure Control Expert
Unity Pro

Resolution:
The likely cause of the SD Card Error was that the card was removed or inserted when the rack was powered up.
This error can be cleared by power cycling the rack or simply removing the BMXNOE0100 from the backplane and reseating it into its slot position.
In both cases, it will power up and get its configuration from the CPU module.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)