Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Problem processing alarm data in the setpoint processor errors in Management Console PME 9.0 System Log Events

Issue:
Power Monitoring Expert server performance is very slow, The System Log Events in PME 9.0 are flooded with Problems processing alarm data in the setpoint processor errors as shown below.

Flood of errors

Product Line:
Power Monitoring Expert 9.0

Environment:
Management Console

Cause:
This is a known issue in PME 9.0. The CU fixed an issue where invalid alarms could cause the alarm processing to stop.

Resolution:
Apply PME 9.0 Cumulative Update 2 (CU2) which can be downloaded from the attached file.





Schneider Electric Saudi Arabia

Attachment(s)
PME 9.0 Cumulative Update 2.zip [120.37 MB]
Power Monitoring Expert 9.0 Cumulative Update 2.pdf [92.53 KB]