Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to apply hotfix from EBO SmartX server (AS/AS-P/AS-B) V3.0+ or higher?
  1. Run the Device Administrator and select the AS/AS-P/AS-B to be upgraded and select the upgrade button, you will be presented with this menu.
  2. Select Apply hotfix and you will be presented with the window as shown below.
  3. Select the OK button and you will be presented with a window to select the hotfix file.
    Locate the hotfix file, i.e. SmartX.Server-3.0.3.11-Hotfix.exe. When the Open button is selected the SmartX server upgrade will begin immediately.
    Warning: if the file fails to load please check the PC has access to the internet as this is required to validate the integrity of the file.
    Note, the hotfix file is a self-extracting archive and will be extracted to the DA folder by DA.
  4. When complete, logon to workstation and verify the running build is correct.