Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you set the two wire type to level control on the ATV600 Process drives?
Issue:
Two wire type to level control on the ATV600 Process drives.

Product Line:
ATV630 and ATV930 Process drives

Environment:
All

Cause:
Set two wire type to level to start on power up with start command

Resolution:
Programming example to set up 2 wire for level control.
Main Menu
Complete Settings
Command and References menu
Set 2-Wire type setting to LEL or Level
Done

ATV600 programming manual
https://www.se.com/ww/en/download/document/EAV64318/

Schneider Electric Saudi Arabia

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: