Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Too many I/O variables using Scadapack Workbench

On certain versions of Windows you may encounter the following error in the output window in SCADAPack Workbench. Too many IO error

The remedy for this challenge is to use the latest Scadapack Workbench version 6.6.10 and perform all software and patch updates to Windows 10. The affected windows version is Win10 64 bits Version 1803 build 17134.1040.

Download

SCADAPack Workbench and Utilities

https://www.se.com/ca/en/download/document/SCADAPack_Workbench/

SCADAPack E Workbench and Utilities

https://www.se.com/us/en/download/document/SCADAPack_E_Workbench/