Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the vertical installation supported for EcoStruxure Building Operation Automation Server (AS/AS-P/AS-B)?

Always install (AS, AS-P, AS-B, I/O modules, and PS-24) on a horizontal DIN rail. This position provides sufficient cooling airflow through the device. Installation on a vertical DIN rail can reduce
the life span of the device.
AS/AS-P:
AS-P installation orientation
AS-B:
AS-B installation orientation