How can we help you today?

Does HMISTO715 support Modbus Function Code 23 in slave mode?

1. Issue
When HMISTO715 is configured as a Modbus slave, is it compatible with Modbus Function Code 23?
2. Environment
HMIST0715
3. Resolution
HMISTO715 supports Modbus SIO Slave Driver and this driver supports Modbus Function Code 23- Read/Write Multiple Registers. So HMISTO715 is compatible with Modbus Function Code 23 in slave mode.
4. FAQ Applicable Conditions
It also applies to HMISTO705 and HMISTO735.

Schneider Electric Saudi Arabia